You are here: Annexes > List of KAS Literature > Installing KAS > Installing Hardware

Installing Hardware

Prior to have your motion application up and running, you first need to connect, wire and configure all your hardware components.

The Getting Started guide contains procedures for installing and configuring hardware components (HMI"Human-machine interfaces " Also known as computer-human interfaces (CHI), and formerly known as man-machine interfaces, they are usually employed to communicate with PLCs and other computers, such as entering and monitoring temperatures or pressures for further automated control or emergency response, PAC"Programmable Automation Controller" PAC is a compact controller that combines the features and capabilities of a PC-based control system with that of a typical programmable logic controller (PLC). A PAC thus provides not only the reliability of a PLC, but also the task flexibility and computing power of a PC. Additionally, because they function and communicate over popular network interface protocols, PACs are able to transfer data from the machines they control to other machines and components in a networked control system controllers, I/O Terminals, EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs Motion Bus, AKD DriveControl device for regulating the speed, torque and position of a motor, and AKM Motor).

Figure 4-1: Connecting all the Hardware components

Links to installation instructions for hardware components can be found in the following table.

Component

Installation

HMI (Human-MachineThe complete assembly of all connected parts or devices, of which at least one is movable Interface)

Install the graphic operator interface

Install HMI

Controller

Industrial PC

Install the Panel or Box Programmable Automation Control (PAC)

Install Industrial PC

EtherCAT Motion Bus

Set up EtherCAT Motion Bus Communication

See AKD™ EtherCAT Communication

I/O Terminal

I/O Modules

Install the remote Input/Output Terminal

Install I/O Terminals

AKD Drive

Drive

Install the AKD Drive

See AKD Installation Manual

(and also AKD Quick Start)

AKM Motor

Motor

Install the AKM Motor

Mechanical and Electrical installation

Available from http://www.kollmorgen.com/

Table 4-1: Kollmorgen Automation Suite Installation and Configuration

 

HMI

PDMM & PCMM

Industrial PC (PAC)

EtherCAT Fieldbus

Remote Input/Output Terminal

AKD Drive

AKM Motor


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™